How do I create a new project in EcoSet Config?
To create and design multiple switchboard, and to configure it , you must create a project. When a new project is created, you can develop multiple switchboards and configure each switchboard with required switchgears.
- Click Create a project.
- Enter your project name and update the basic information.
- Select the latest price list from the Applied price list drop down menu.
- Click Create.
Your new project is now created, and you can proceed to create a new switchboard.
The following tabs will appear in sequence.
| Tabname | Function |
| MANAGESWITCHBOARD(A) | To manage multiple switchboards for a project. |
| SELECTAPRODUCT(B) | To create and manage switchboards. |
| SINGLE LINE DIAGRAM (C) | To generate and view the single line diagram. |
| DESIGN A SWITCHBOARD (D) | To select and manage switchboards. |
| BILLOFMATERIAL(E) | To generate bill of material for the final products. |
| EXPORT(F) | To export all project related documents in different document format like pdf, csv, jpg. |
Manage Switchboards