Hôm nay chúng tôi có thể giúp gì cho bạn?

Can't configure IEC61850 in P30

Issue

Recently we received some BFO cases where customer don’t know how to configure IEC61850 in P30 relay.

11

_____________________________________________________________

Product Line

P30

_____________________________________________________________

Environment

All firmware

_____________________________________________________________

Phenomenon

MCL 61850 and CID 61850 Folder are grey color and can’t be configured.

_____________________________________________________________

Root Cause

It is needed to enable IEC61850 ed1 or ed2 first and refresh the connection.

_____________________________________________________________

Solution

Enable IEC61850 ed1 or ed2 first.

1

Then refresh the connection.

2

Then we will see MCL61850(ed1) or CID61850(ed2) folder is ready for configuration.

3