Hôm nay chúng tôi có thể giúp gì cho bạn?

Compact DAP204 to X80 DRA0804/0815 quick wiring - 990XSM00203

Issue

Migrating an ASBDAP204 to a BMXDRA0804/0815 and need to confirm the 990XSM00203 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout