Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to print the logic of a project in Control Expert?

Article available in these languages: Tiếng Tây Ban Nha

Issue:

This FAQ explains the steps to print the project logic and provides tips for better organization.

Product:

EcoStruxure Control Expert (previously Unity Pro)

Environment:

PLC Configuration Software in Windows

Resolution:

To print the logic to a PDF, follow the steps shown in the image below:

1

Note: You can select which sections you want to print. In this example, all sections were selected.

2

Unfortunately, we are limited to a certain number of columns and rows (space) per page type. You can adjust the page setup and margins to fit as much of the logic as possible:

3

4

You can also enable Page Breaks to view how each page is divided. This feature helps you understand what content will appear on each page:

5

6

7

These are the available features you can use when working with the project printout.