Hôm nay chúng tôi có thể giúp gì cho bạn?

Font compatibility between Vijeo Designer Editor and its different targets

Issue:

This FAQ explains which fonts are compatible with Vijeo Designer and its different targets, as well as how to add additional fonts for IPCs.

Product:

Vijeo Designer v6.2, v6.3

Environment:

HMI Configuration Software in Windows

Resolution:

  • Non-windows HMIs:

Depending on the target used, the available fonts will be fixed. For non-Windows HMIs, you can find the list of compatible fonts in the help guide:

1

2

You cannot add fonts here.

  • Industrial PC (IPC)

If you use an IPC target in Vijeo Designer, the fonts displayed will be those available in Windows:

3

If you want to add more fonts, you need to install them on your windows IPC.

Also, keep in mind that the IPC must have the same fonts as the PC where you created the project.