Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is EcoStruxure Machine SCADA Expert v2023 compatible with the HMIG5U21?

Issue:

Can Machine SCADA Expert v2023 run correctly in the Harmony GTU HMI open box HMIG5U21?

Product:

  1. EcoStruxure Machine SCADA Expert v2023
  2. HMIG5U21

Environment:

  1. HMI Configuration Software in Windows
  2. Harmony GTU HMI open box with Windows 10 IoT

Resolution:

Short answer: In theory it is compatible but it is not recommended.

EcoStruxure Machine SCADA Expert v2023 have the following requirements:

From: EcoStruxure™ Machine SCADA Expert , Help Manual - 07/2024 - P.38

1

The HMIG5U21 barely meets these requirements:

From: HMIG5U21 product data sheet

2

Note: Keep on mind that the actual available memory might be less than 4 GB, especially if the OS and other tasks are running.

From: Harmony GTU, User Manual - 01/2022 - P.12

3

The HMIG5U21 is theoretically compatible with EcoStruxure Machine SCADA Expert v2023; however, it is not recommended for Machine SCADA Expert applications. Machine SCADA Expert projects are typically complex and may require even more system resources.

Related resources:

Title: EcoStruxure™ Machine SCADA Expert, Help Manual

URL: https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000002448&p_enDocType=User+guide&access=Public

Title => "Harmony GTU, User Manual"

URL => https://download.schneider-electric.com/files?p_Doc_Ref=EIO0000001735&p_enDocType=User+guide&access=Public

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Phạm vi:
Tìm hiểu thêm
Sản phẩm: