Hôm nay chúng tôi có thể giúp gì cho bạn?

Reasons for "Your account has been disabled" in Secure Connect Advisor

Issue:

Users may encounter the error message:

Login Failed - Your account has been disabled

1

when attempting to log in to Secure Connect Advisor - Gate Manager.

Product:

EcoStruxure™ Secure Connect Advisor (formerly known as Vijeo Connect)

Environment:

Secure Remote Access Software in Windows

Resolution:

1- User Account Disabled in Gate Manager

The account being used may have been disabled within the Gate Manager.

To verify this:

  • Log in with an administrator account.
  • Navigate to Users and check the status of the account.
  • If disabled, enable the account and save changes.

Example when account is disabled:

2

3

When trying to log in to the Gate Manager:

4

2- License Expired

If the Secure Connect Advisor yearly subscription-based license has expired, the account will be disabled. To restore access, you must renew the subscription license.