Hôm nay chúng tôi có thể giúp gì cho bạn?

Power Monitoring Expert (PME) 2024 Trial License

Issue

Does Power Monitoring Expert (PME) 2024 have a trial license?

Product Line

Power Monitoring Expert 2024

Environment

PME License Configuration Tool

Cause

Changes to the PME 2024 licensing.

Resolution

The embedded 90 day trial license in PME 2024 or newer versions is valid until December 31, 2025. From January 1, 2026 and on, a fresh installed PME 2024 will not have any trial license.

Example:

  • If PME 2024 is freshly installed on October 14, 2024, PME 2024 can run under its embedded trial license until January 12, 2025
  • If PME 2024 is freshly installed on January 1, 2026, PME 2024 cannot run on its embedded trial license as it has expired. A full license of PME 2024 will be required

Recommendation
If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo-psup@se.com

Upgrade details