Hôm nay chúng tôi có thể giúp gì cho bạn?

Ordering Guidelines for the MiCOM P992 Multi Finger Test Plug

Issue

Clarification is needed on how to order the MiCOM P992 multi‑finger test plug

Product

MiCOM P992 Test Plug

Environment

Protection relay testing environments requiring a universal multi‑finger test plug compatible with MiCOM relay test interfaces.

Cause

Uncertainty exists regarding the correct ordering code and model availability for the MiCOM P992 test plug.

Resolution

The MiCOM P992 is a single universal multi‑finger test plug model designed for compatibility with any P991 test block of MiCOM test interfaces.

The correct part number for ordering this plug is E992C.

It can be ordered through our Authorized distributors (find one near you here). They will contact Schneider Sales Support team for a direct quotation since this part is not registered in the system as a standard item.

1