"Software Protection Failure. No key found or no license available from network" System services "Login Aborted" in service mode
Issue
Running Power Operation in service mode results in the below error.
Product Line
Power Scada Operation 2020
Power Scada Operation 2020 R2
Power Scada Operation 2021
Ecostruxure Power Operation 2022
Ecostruxure Power Operation 2024
Environment
Windows Services
Setup Editor
License Configuration Tool
Runtime Manager
Cause
Autologin mode being disabled is necessary in order to have the service account run the Runtime Manager. With autologin mode disabled, a login form is generated which the service cannot enter the credentials for. This causes the system to hang and login to be aborted.
Resolution
Reference the [Client]AutoLoginMode parameter to make the best decision for how to start the Runtime Manager. If Power Operation is to be run in service mode, it is best to run in AutoLogin Mode.