Hôm nay chúng tôi có thể giúp gì cho bạn?

PME - Does PME support Change Data Capture (CDC) on its SQL Server databases?

Issue

Does PME support Change Data Capture (CDC)?

Product Line

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

SQL Server

Resolution

PME does not currently support Change Data Capture (CDC).

The PME installer and Configuration Manager tool will encounter SQL errors when attempting to restore backups of CDC-enabled databases.