Hôm nay chúng tôi có thể giúp gì cho bạn?

EAE25.0: How to enable Secondary NTP server for DPAC Controllers(ATV, M251, M262, M580)

This knowledge base article explains users on How to enable Secondary NTP server for DPAC Controllers (ATV, M251, M262, M580).

By default, User can find only Primary NTP server Configuration in Device Settings as shown in the below screenshot.

ntp1

In order to get the secondary NTP server configuration, User needs to select "Advanced" in Generic settings of Automation Expert Software as shown in below Screenshot.

ntp2

This setting will make other Device configuration settings also visible along with Secondary NTP server Settings and you can enable the Secondary NTP server as shown in below screenshot.

ntp3