Hôm nay chúng tôi có thể giúp gì cho bạn?

Smart UPS Modular Ultra has an IM alarm after toggling the system enable switch

Issue:

Customers may experience IM (Intelligence Module) alarms, IM not operating properly, or similar alarms after toggling the System Enable switch on the back of the system. These alarms may not clear on their own, even after returning the switch to its normal position.


Product Line:

Smart UPS Modular Ultra


Environment:

All models, all serial numbers


Resolution:

Perform a full power cycle of the system to clear the IM fault condition and restore normal operation.

Follow the power cycle procedure FAQ here:
https://www.se.com/us/en/faqs/FAQ000274118/

Notes

  • This behavior can occur with various IM-related faults, not tied to a specific alarm code.
  • Symptoms may include:
    • IM fault alarms
    • IM not operating properly
    • Unexpected IM communication or status issues
  • If alarms persist after a complete power cycle, please reach out the technical support.
The System Enable (SE) switch should only be used when required for service or troubleshooting activities. Avoid repeatedly toggling the switch and allow the UPS to fully complete its startup and initialization process after re-enabling the system. Improper or repeated use of the SE switch may result in temporary Intelligence Module (IM) initialization alarms during system startup.