Hôm nay chúng tôi có thể giúp gì cho bạn?

What is maximum rating of the "MVLV transformer" defined at the EcoSet Design?

EcoSet Design allows the MV/LV transformer ratings upto 2500 kVA to ensure safe, reliable, and Standard compliant LV distribution, while maintaining proper protection coordination and manageable fault levels.

This limit is established in line with standard engineering practices for low-voltage (LV) distribution systems, considering:

  • Switchgear and busbar limitations at LV level
  • Manageable short-circuit (fault) levels
  • Efficient protection coordination
  • Compliance with relevant standards.