Hôm nay chúng tôi có thể giúp gì cho bạn?

Upgrading NetBotz NBRK0250A to version application version 3.4.2.6 no longer allows Rack access door renaming.

Issue:
Upgrading NetBotz NBRK0250A to version application version 3.4.2.6 no longer allows Rack access door renaming.

Product Line:
NetBotz

Environment:
NBRK0250A version 3.4.2.6

Cause:
An issue with version 3.4.2.6 firmware does not allow doors to be renamed in the same way other sensors might

Resolution:
Engineering is looking to resolve this in a future revision of firmware.