Hôm nay chúng tôi có thể giúp gì cho bạn?

Machine Expert 2.3 Password Expiration: Default Setting and Configuration

Issue:

We have a customer whose HMI was disconnected from their machine due to the Password Expiration setting that was introduced in Machine Expert 2.3 and 2.5.

We understand that this feature can be disabled in the Machine Expert settings; however, we have been unable to determine the default expiration period when the setting remains unchanged from its default value.

Product Line:

EcoStruxure Machine Expert version 2.3 and above.

Resolution:

To confirm the default value for the Password Expiration TimeoutDays that is configured in a specific Machine Expert controller,

it is required to connect to the specific controller for which this value has not been changed.

Once connected to the controller, follow the steps given in the FAQ:

https://www.se.com/my/en/faqs/FAQ000282281/

Access the Password Expiration TimeoDays parameter and confirm the value.

For the M241, M251 and M262 controllers, the default value is 365 days. It is possible to change it from 0 to 1000 days.

Password Expiration parameters.

NOTE: For Machine Expert v2.3 and 2.5, the Password Expiration parameter was set to Enabled by default. Starting with version 2.6, it is now set to Disabled.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)