Hôm nay chúng tôi có thể giúp gì cho bạn?

Can I show or hide individual current markers in EcoSet Design Curve Part ?

Yes.

In the Current tab of the Curve window, users can show or hide individual current markers by selecting or clearing the corresponding checkboxes. This provides greater flexibility when analyzing specific current values and improves curve readability.

For example, users can choose to display only:

  • Design Current (Ib) for load verification.
  • Fault Current for short-circuit analysis.
  • Earth Fault Current for earth fault studies.
  • All Current Markers for a complete selectivity and protection review.

This feature allows users to focus on the most relevant current indicators based on their analysis requirements.

labels