Hôm nay chúng tôi có thể giúp gì cho bạn?

Can users control the startup tutorial in EcoSet Design?

Yes. EcoSet Design includes a Self-Guided Tour that helps users become familiar with the application and its recommended workflow. When a project is opened for the first time, the tour provides step-by-step guidance through the main features and functions of the software.

turorial

Key Features

  • Interactive walkthrough of the EcoSet Design interface and key functionalities.
  • Numbered guidance aligned with the recommended project workflow.
  • Assists users in creating, configuring, calculating, and documenting projects.
  • Can be launched at any time from within the application for additional guidance or refresher training.

User Control Options

Users can decide whether the Self-Guided Tour is displayed automatically when opening future projects:

  • Enabled: The tour is displayed at startup.
  • Disabled: The tour is not shown during subsequent application launches.
  • The setting can be changed at any time, allowing users to re-enable the tour whenever needed.
  • We can click End Tutorial button to close the tutorial tour.

Key Benefits

  • Accelerates onboarding for new users.
  • Improves understanding of application features and workflows.
  • Provides contextual, in-application guidance.
  • Helps users become productive more quickly and efficiently.
  • Offers flexibility for both new and experienced users by allowing the tutorial to be enabled or disabled as required.

Note: The Self-Guided Tour serves as a built-in learning tool, enabling users to explore EcoSet Design's capabilities at their own pace while maintaining full control over when the tutorial is displayed.