Hôm nay chúng tôi có thể giúp gì cho bạn?

How do I run calculations in EcoSet Design?

To perform electrical calculations:

  1. Complete the Single Line Diagram (SLD).
  2. Define the source, protection devices, cables, and loads.
  3. Select Run Calculations from the toolbar.
  4. Review the calculation status in the Notifications panel.
  5. Analyse the results in the Results panel.

The software calculates:

  • Load currents
  • Cable sizing
  • Voltage drops
  • Short-circuit currents
  • Protection device coordination
  • Selectivity

run