Hôm nay chúng tôi có thể giúp gì cho bạn?

Can I modify the order of properties displayed on the SLD in EcoSet Design?

Yes. The order of properties in the Properties Selected panel determines how information is displayed on the Single Line Diagram (SLD).

To improve readability, users can rearrange properties and place the most important information at the top of the label. Once saved, the updated order is reflected on the diagram.

labels