Hôm nay chúng tôi có thể giúp gì cho bạn?

How do I configure and use Harmony XB5R/XB4R wireless pushbuttons?

1. What you need to know

Harmony XB4R (metal) and XB5R (plastic) pushbuttons are wireless and battery less: pressing the button generates the energy needed to send a radio frame to the receiver, which converts it into an output for a PLC input or a control circuit. No wiring and no battery maintenance are required. Configuration consists of pairing each transmitter with a receiver channel, then selecting the output mode.

2. How it works and how it is set up

The range is built on energy harvesting: the mechanical action of the operator generates the energy for one radio transmission. Only the receiver is wired and powered.

  • Each transmitter sends a unique identifier, so a receiver only reacts to the transmitters paired with it.
  • Transmitters can be mounted on moving or remote parts of a machine where cabling is impractical.
  • Pairing and output settings are stored in the receiver and survive a power loss; output states do not.

See each configuration step below:

  1. How to pair and unpair a Harmony ZBRT1 or ZBRT2 transmitter?
  2. How to configure a Harmony ZBRRA receiver?
  3. How to duplicate an electrical function using Harmony XB5R?
  4. How to lock and unlock a Harmony ZBRRA or ZBRRC receiver?
  5. How to replace a Harmony ZBRT1 or ZBRT2 transmitter?
  6. How to reset a Harmony ZBRRA and ZBRRC receiver?
  7. How to adjust your equipement using ZBRT2 transmitters?
  8. How to Install ZBRV1 on ZBRT to receive visual feedback

NB : ZBRRD has been discontinued since June 2026.

3. Choosing the receiver

CriterionZBRRAZBRRC
Output type2 changeover relays, 3 A4 PNP solid-state, 200 mA
Supply voltage24…240 V AC/DC24 V DC
Output modesMonostable, Bistable, Enable/DisableMonostable

4. Schneider Electric references

FunctionReferenceDescription
Receiver, relay outputsZBRRA2 changeover relay outputs 3 A, 24…240 V AC/DC
Receiver, solid-state outputsZBRRC4 PNP outputs 200 mA, 24 V DC
TransmitterZBRT1Wireless and battery less transmitter, without head, simple action
TransmitterZBRT2Wireless and battery less transmitter, without head, double action
TransmitterZBRV1Visual feedback for ZBRT transmitters
AntennaZBRA1Relay antenna to extend radio range

Launch Product Selector on se.com to configure a Harmony XB4R or XB5R solution or contact Schneider Electric Technical Support.