Hôm nay chúng tôi có thể giúp gì cho bạn?

EAE26.0 : How to open weblinks from EAE Windows HMI

This knowledge base article explains users on how to open weblinks from Ecostrusure Automation Expert HMI.

  1. Take a Button on to the HMI Canvas and name it as WebLink as shown below.

w1

2. Double Click on the added button to open C# source code and Once C# code opened, make sure “System.Diagnostics” library is referenced if not then add it manually as shown below.  .

w2

3. Locate the button name as shown below .

w3

4. Under that, kindly write the function, Process.Start("URL"); command for added button to open URL as shown below. In this example we are opening the weblink "https://www.se.com/in/en/product-range/23643079-ecostruxure-automation-expert/"

w4

5. Build and then RUN the HMI. Upon clicking the button the website will be opened. Kindly note that this will work with only Windows HMI Projects.