Hôm nay chúng tôi có thể giúp gì cho bạn?

How to resolve “Bits number (%I,%M) must be aligned on paragraph of 128 bits” after upgrading the M580 firmware in a project?

Issue:

After upgrading the M580 firmware version configured in EcoStruxure Control Expert, the following error may be reported during a project build:

Parameter <Number of outputs bits> in error (RIO bus S908 Support in M580: the Bits number (%I,%M) must be aligned on paragraph of 128 bits (and >=128))

2

This error may appear when upgrading a project from an M580 firmware version prior to v2.30 to a higher version.

This issue applies only to M580 PLCs that support S908 drops.

Product:

M580 controller

Environment:

EcoStruxure Control Expert software (previously Unity Pro)

Resolution:

Verify the configured size of the %I and %M State RAM areas.

Starting with M580 firmware v2.20, the number of bits must be 128 or greater and aligned to a multiple of 128 due to changes implemented to the S908 memory usage.

Adjust the affected memory size to an appropriate multiple of 128.

Example:

If %M is configured to 1008, it is not correctly aligned. Change the value to 1024, which is a multiple of 128.

1

After changing the memory configuration, the project can be rebuilt without errors.

Note: Transferring the rebuilt project will require the PLC to stop.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)