What are the adjustment ranges for the dials on an ATS01N1..FT?
What are the adjustment ranges for the dials on an ATS01N1..FT?

Issue :
Adjustment ranges for Schneider-Electric recommend for Altistart Soft Starters?

Product Line :
Altistart Soft Starters

Environment :
Open style Soft Starters

Cause :
Adjustment Range

Resolution :
For the START TIME dial, setpoint A is 1second and setpoint E is 5seconds.  There is a linear relationship from A to E setpoints.
For the INITIAL VOLTAGE dial, setpoint A is 30% and setpoint E is 80% of full voltage.  There is a linear relationship from A to E setpoints.

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: