Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Video: How to create customized screens for the CM4000 display
Issue
What is the best method for creating customized screens for the CM4000 display

Product Line
CM4000

Environment
Meter Display Configuration

Resolution
Custom displays can be programmed using the meter's remote display. There is no remote software support for local display screen development.

For instructions on how to set up these customized screens please see the CM4000 reference manual which is attached below. The instructions for setting up custom screens begin on page 35.

Here is a video which shows how to setup custom screens and view them via front display:

Schneider Electric Česká republika

Přílohy
CM4000_Reference_Manual.pdf [3.41 MB]