Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Are the ION meters seismic and/or vibrational compliant?

As of right now, no ION hardware undergoes any testing for seismic and/or vibrational compliance. No meters in the ION family have this compliance. Typical standards are IEEE 693 and IEC 60255-21-3.
________________________________________
Original article#
Date Created: November 12, 2010
Last Revised: November 18, 2010
Public
Original Author: DD
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL203933 V1.0, Originally authored by LaAd on 11/19/2010, Last Edited by LaAd on 11/19/2010
Related ranges: ION8600, ION75X0 RTU, ION7550/ION7650, ION7300, ION6200