Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What are the three methods of connecting to the ConneXium Firewall? (Part# TCSEFEC23F3F20)

Goals and Symptoms

What are the three methods of connecting to the ConneXium Firewall?

Causes and Fixes:

The device has three user interfaces, which you can access via different
interfaces:

  • 1. Web-based interface via Ethernet (SNMPv3, in-band)
    2. System monitor via the V.24 interface (out-of-band)
    3. Command Line Interface (CLI)
    • via the V.24 connection (out-of-band)
    • via SSH (in-band)