Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Transferring authorization from disk to computer returns 'COMPNO NOT FOUND' error.
Issue
Transferring authorization from disk to computer returns 'COMPNO NOT FOUND' error.

Product Line
ProWORX 32

Environment
Windows XP Professional, ProWORX 32

Resolution
If you try to transfer the authorization using the option ' transfer authorization from disk to computer, the ' 'COMPNO NOT FOUND' error could get returned.
CDc

The error can be ignored.  If you click on OK and then click on Next, it will show that the software is already authorized.
scdcd
  • Click on 'NO'.
  • Click on Cancel.
  • Restart ProWORX 32.