What is the address of the com scanner input/output tables on the ATV630 Process Drive?
Issue:
Com scanner address input/output tables on ATV630

Product Line:
Altivar Process drive.

Environment:
All models, All serial numbers.

Cause:
Information not available in current literature.

Resolution:
Com scan IN value 1:     12741 dec
Com scan IN value 8:     12748 dec
Com scan OUT value 1:     12761 dec
Com scan OUT value 8:     12768 dec

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: