What is the latest released version of the (MBX Driver Suite) Modbus Plus Driver?
Issue:
Information for the MBX Driver Suite
Environment:
MBX Driver Suite V9.0
Part# SWMXDS001
Resolution:
This driver is delivered with the following products:
416NHM21234
TSXCUSBMBP
416NHM30042A
Version 9.0 supports:
Windows 10
Windows 8
Windows 7 SP1
Windows Server 2016
Windows Server 2012
Windows Server 2008 R2 SP1
NOTE: Please contact Sales for information on purchasing a device driver.