Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Com'X system has been configured with fast logging (less than 15 min logging interval ) with many topics on many devices, the device is very slow, why?
The device performance has degraded, to many data to manage in time, all monitoring data are needed ?
We recommend  to reduce the  logging interval frequency (> or = 15min.) or reduce the amount of data being logged.
In the future the Com’X will come with a tool to help assess optimum configuration.