Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Why a bandwidth limitation on the service port of 140NOC78xxx?
Issue

Why do we have a limitation on the service port of a 140NOC78x00?

Product Line

Quantum

Resolution

Servicing the service port (low priority) slows down the process of servicing the control port (high priority); to resolve the latency that can be caused by the traffic from the service port toward the traffic on the control port, a limitation is set on the service port.