Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What are the character limitations of Advanced Meter Security passwords

Issue

Power Monitoring Expert and related advanced meters may show signs of security errors through the system log found in the Management Console or in the Web Application

Product Line

ION Setup

ION8300

ION8400

ION8500

ION8600

ION8650

ION7650

ION7550
ION9000

ION7400

PM8000

Environment

Advanced Meter Security

Resolution

Passwords containing numeric only characters can be a maximum of 8 characters in length.

Passwords containing non-numeric characters can be a maximum of 6 characters in length.

Note: The passwords should not contain any characters from the extended ascii table, such as accented letters, or characters from languages other than English.

Restrictions and password requirements for authentication on ION meters.

1. Numeric (0 - 99999999); The password may have a length of up to 8 numerical digits only.

2. No spaces are permitted.

3. No leading zeros followed by other numerical digits.

4. Valid ASCII characters only.

5. Passwords that are alpha, alphanumeric and/or includes symbols are limited to 6 characters only.


Valid examples of ION meter passwords:

User1 password: 0  (zero)

User2 password: 12345678 (this is the longest allowed numeric password at 8 digits)

User3 password: 0A123  (old alphanumeric style)

User4 password: #A134  (new style with non-alphanumeric character)

User5 password: 01234$  (looks numeric but has additional non-numeric character)

User6 password: A^@g5  (strongest possible with upper/lower case, symbols and numeric digits)