Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can a Quantum IO module be hot swapped?
Yes. However this must be done by a qualified individual who is familiar with the inputs or loads associated with the module.
You need to be aware of how the loss of signal input or control output can effect the application.\ before performing the swap.

Quantum CPU's should never be hot swapped.
Don't hot swap a stand alone power supply in the main PLC rack as it will result in a corrupted project.



R-72417