Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do I configure network settings on my Symmetra PX 250/500 UPS?
Issue:
Video: How to Configure network settings

Product line:
Symmetra PX 250-500

Environment:
All Product models, all serial numbers

Cause:
How do I Configure network settings  on my Symmetra PX 250-500 UPS

Resolution:
Begin at the home screen of the UPS
Press the wrench key at the lower left of the screen
Select Configuration then User configuration
Enter the user password (apc by default)
Select NMC settings
Select Configure NMC Settings on the card you would like to configure.
Ensure the ‘UPS configuration access’ is set to read or read/write for the card
Make desired changes and Select Apply to save changes.

See the following video tutorial:

1 IFramehttps://www.youtube.com/watch?v=_gfDhRQs6Z4&ab_channel=SchneiderElectric