Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Video: Viewing PowerLogic ION Power Meter Phasor Diagrams in ION Setup

Issue
Request to view the phasor diagram on an ION meter

Product Line
ION7000 series
ION8000 series
PM8000 series

Environment
ION Setup

Resolution
In order to view the phasor diagram with ION Setup, follow the steps below:

  1. Connect to the meter using ION Setup.
  2. Open Setup Assistant from the right pane of the screen.
  3. Click on Verification.
  4. Click on the Wiring tab.
  5. Click on phasor viewer then click on Confirm.
  6. The phasor diagram is then displayed.


The following video demonstrates this procedure: