How do I program the ATV630 for +/- speeds via digital inputs?
Issue:
Programming reference switching and +/- speeds via digital inputs for the ATV630.

Product Line:
Process Drives

Environment:
ATV630  ATV930

Cause:
Setup +/- speed as second reference.

Resolution:
[Complete settings] [Command and Reference]
Freq Switch Assign =  Ref Freq Channel 2
Ref Freq 2 Config = Ref Frequency via DI

[Complete settings] [Generic functions] [+/- speed]
[+ Speed Assign] USP = desired DIx  Increase speed input assignment.
[- Speed Assign] dSP = desired DIx  Down speed input assignment.

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: