SoMachine Configuration Manager Version 433.18.34401 This installer introduces the update of the License Manager integration to enable the registration with the newest version of the License Server. This version is needed to be installed before introducing following new SECO files for SoMachine Motion V4.0 and V4.1 and SoMachine V4.1 Related SECO files: SoMMV4.0_TLS1.2_AddOn_4.0.0.0_21.07.30.1.seco SoMMV4.1_TLS1.2_AddOn_4.1.0.0_21.07.30.1.seco SoMMV4.2_TLS1.2_AddOn_4.2.0.0_21.07.30.1.seco SoMV4.1_TLS1.2_AddOn_4.1.0.0_21.07.30.1.seco SoMV4.1_SP2_TLS1.2_AddOn_4.1.0.1_21.07.30.1.seco
Fecha:
13 ago 2021| Tipo:
Software
idioma:
Inglés| Versión:
V433.18.34401
Sistemas operativos:
Windows 10, Windows 8
Referencia del Documento:
SoMachineConfigurationManager
Para acceder al documento
Crear una cuenta
o
Ingresa