Preguntas frecuentes de búsqueda
Does the ATV12 drive have a type 1 conduit kit option?
Issue:
Nema type offered for the conduit kit on an ATV12
Product Line:
ATV12, Altivar 12
Environment:
All
Cause:
Nema 1 rating kit.
Resolution:
The ATV12 drives does not have a Nema 1 conduit kit option available.
There are covers over the input and output power terminals, but this does not meet the NEMA 1 requirements.
The VFD should be mounted inside a separate enclosure.
Publicado para:Schneider Electric España
Documentos adjuntos
Explorar más
Rango:
Explorar más
Rango: