Hae usein kysyttyjä kysymyksiä
What type of power fuse is required for the 8930 Irrigation Field Drive?
Issue:
Power fuse for the 8930 Irrigation Field Drive?
Product Line:
8930 IFD Field Drive
Environment:
All models
Cause:
Power fuses are not included with the Field Drive
Resolution:
See the attached file excerpt from the Instruction Bulletin, 30072-454-01.
Locate the fuse type based on the Field drive power voltage, HP and variable/constant torque.
Power fuse for the 8930 Irrigation Field Drive?
Product Line:
8930 IFD Field Drive
Environment:
All models
Cause:
Power fuses are not included with the Field Drive
Resolution:
See the attached file excerpt from the Instruction Bulletin, 30072-454-01.
Locate the fuse type based on the Field drive power voltage, HP and variable/constant torque.
Julkaistu:Schneider Electric Suomi
Liitteet
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: