Kuinka voimme auttaa sinua tänään?

Is it possible to extend the distance between BCPM CTs and the adapter board?

It depends on which CT's your are referring to. The split-core branch CT leads can be extended to a maximum length of 6 meters without losing accuracy.
The 1VAC AUX CT leads can be extended to 30.5 meters.