Kuinka voimme auttaa sinua tänään?

How to deactivate the User Rights only for the Web Visualization on M241/251 and M262 controllers?

From EcoStruxure Machine Expert V2.0, it is now possible to deactivate User Rights for the Web Visu only on M241/251 and M262 controllers.
It means User Rights remain active for other services.

To do that, User must create the empty file WebVisuNoLogin.cfg into the folder /usr/Visu and reboot the controller.

After this action, no password is required to connect to the web visualization.

WebVisuNoLogin.cfg file can be downloaded to the controller through FTP Server connection or from EcoStruxure Machine Expert (MyController >> Files tab).


Through FTP Server connection:
FileZilla


From EcoStruxure Machine Expert:
Machine Expert