Kuinka voimme auttaa sinua tänään?

L-shape combination of switchboard

Based on the switchgear room layout, enclosures needs to be arranged in a way that it fits in the switchgear room. One such combination is in L-shape combination in PrismaSeT I.

Enclosures can be combined in L-shape or at right angles using IP30 right angle kit as shown in below image.

L-shape 1

Fig. 1

It should be noted that the busbar needs to be cut as per specified dimensions and arranged as per below image using fish plates. Please refer to the latest files in TTF.

l shape 2

Fig. 2