Kuinka voimme auttaa sinua tänään?

NLP status on an ATS480

NLP indicates that the unit has no run command, and no main power supplied on L1/L2/L3.

On this softstart, CL1 and CL2 will be needed as hot and neutral 120V control power. With only this power supply provided, the unit will state NLP.