What is the equivalent copper ground bar for a PK15GTA aluminum ground bar?
Is there a copper ground bar for a PK15GTA aluminum ground bar?
Product Line:
Panelboard, Load Center
Environment:
Panelboard, Load Center
Cause:
Product Selection
Resolution:
80103-026-52 is the copper ground bar eqivalent to the PK15GTA which is an aluminum ground bar.