¿Cómo podemos ayudarte hoy?

What is the wire bending space for the Main Service Wires of a 125amp Max., QO or Homeline Load Center?

Issue:

Product Design Features

Product Line:

QO and Homeline Load Centers

Environment:

Mains Wire bending space

Cause:

Information or application

Resolution:

The wire bending space is determine from the UL standards and the NEC, based on the mains amperage rating and maximum wire size the load center will accept. SEE THE NEC wire bending tables.

ALL the 125amp QO(Single phase ONLY) and Homeline Main Breaker and Main Lug Load Centers meet the appropriate wire bending space requirements Per UL and NEC.

The 125amp QO(Single phase ONLY) and Homeline Main Breaker and Main Lug Load centers will have approximately 6.50 to 6.87 inches from the Top endwall down to the top surface of the Mains lugs.