Veelgestelde vragen (FAQ's) zoeken
What replaced XPSAL? What are the differences between XPSAL and the new XPSAC?
XPSAL Replaced by XPSAC
XPSAL (older model) XPSAC (newer model)
- XPSAC has one extra N/O safety output
- XPSAC has a solid state output for PLC signaling
- XPSAC has choice between 2 models with or without removable plug terminals (P)
Schematic Comparisons
Monitoring of E-stop with 2N/C contacts
Monitoring of E-stop with 1N/C contact
Cross Reference Table
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie