Veelgestelde vragen (FAQ's) zoeken
What are the dimensions of the metal guards, part number ZBZ1600, for the emergency stop function?
Concerning the following part numbers:
The dimensions of the metal guards for the XB4 and XB5 ranges of diameter 22 emergency stop pushbuttons are as follows:
- ZBZ1600 PB Mushroom Guard Chromium plated
- ZBZ1602 PB Mushroom Guard Black
- ZBZ1604 PB Mushroom Guard Red
- ZBZ1605 PB Mushroom Guard Yellow
- ZBZ1606 PB Mushroom Guard Blue
The dimensions of the metal guards for the XB4 and XB5 ranges of diameter 22 emergency stop pushbuttons are as follows:
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie