Veelgestelde vragen (FAQ's) zoeken
Why can't I transfer an application between the PC and the XBTN or XBTR terminal using the TSXCUSB485?
Context:
Possible solutions:
Note:
- The objective is to import or export an application to or from one of the following types of XBT terminal: XBTN200, XBTN400, XBTR400, XBTRT500 or XBTRT511.
- The PC is connected to the XBT terminal via the TSXCUSB485 converter and the XBTZ925(A) cable.
- The XBTL1000 displays the message "No terminal connected",
- or Vijeo Designer Lite displays "No terminal connected".
- The XBT terminal does not display the message "Waiting for transfer" but shows the error message #204 "Connection in progress".
Possible solutions:
- Disconnect the XBT-Z925(A) cable and reconnect it the other way round, as it has two cable ends which are not symmetrical.
- The XBT terminal should then display the message "Waiting for transfer".
- Check that the Uni-Telway driver installed on the PC is definitely assigned to the corresponding COM port on the TSXCUSB485 converter.
- The rotary selector switch on the TSXCUSB485 cable must be set to 0 or 1.
Note:
- The position of the "Polarisation" selector switch on the TSXCUSB485 converter is not relevant to communication.
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie