Veelgestelde vragen (FAQ's) zoeken
Can a Modbus protocol be used to communicate between a Micrologic and a TSX PLC?
Yes, Modbus communication is possible between a Micrologic and a TSX PLC. For an NT, NW or compact NS 800 to 3200 plug-in circuit breaker, the data tables are divided into 4 managers (3 for a fixed circuit breaker).
The four addresses (or the 4 slaves with linked addresses) are:
The four addresses (or the 4 slaves with linked addresses) are:
- @ xx for the circuit breaker manager
- @ xx +50 for the "chassis" manager
- @ xx +100 for the "protection" manager
- @ xx +200 for the "measurement" manager
Note: This platform is discontinued. Please get access to our digital catalog https://digicat.se.com/ or contact our support center for more information about migrations to a newer platform. |
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Ontdek meer